Please select your country

STULZ worldwide

Space-saving split air-con saves energy for server rooms

EC Tower

STULZ’s new EC Tower, is designed for rapid deployment and requires a third of the footprint of some conventional precision air-conditioning units.

Temperature management for IT infrastructure is critical, even for smaller server and technical rooms, and precision air-conditioning is vital. To meet this demand, a new split air-conditioning system – the EC Tower – has been launched by STULZ UK, offering high levels of reliability and precision control, in a fraction of the footprint of conventional air-conditioning systems.

“All too often, poorly specified cooling technology leads to erratic climate control, increased operating expenditure and costly disruption to IT operations. Downtime is not an option regardless of the size of the server room. However, precision cooling solutions, such as the EC Tower series, are ideally suited to technical spaces that cannot compromise on reliability, space or cost,” comments Phil McEneaney, Head of Sales, STULZ UK.


Reduced energy costs

The EC Tower series combines the proven reliability of STULZ's precision air-conditioning technology with the advantages of modern inverter outdoor condensing unit. A split climate solution, the EC Tower range can be rapidly deployed for heat loads of 5kW to 24 kW. A key advantage of the outdoor condensing unit is the ability to support dynamic capacity adjustment of the rated cooling capacity – which delivers significant energy savings.

“For SMEs this is an important consideration – energy efficiency is high on the agenda from a corporate responsibility perspective, but it also improves the bottom line,” McEneaney adds. The EC Tower series is designed for continuous, 24/7/ cooling of technical rooms. While conventional comfort air-conditioning units can use up to 40% of their cooling capacity in dehumidification, the EC Tower generates between 90% and 100% of sensible cooling capacity which reduces dehumidification and lost performance. The high Sensible Heat Ratio (SHR) value eliminates problems associated with removing moisture via the evaporator which can be an issue in technical environments, causing static build up within the technical equipment.

An additional benefit of the EC Tower is the increased distance between the internal and external condensing unit of up to 100 metres which enables flexible installation.


Space-saving solution

“We have listened to the needs of customers and developed a space-saving solution that offers the benefits of easy installation and precision control,” concludes McEneaney. When space is at a premium, this configuration will prove ideal for end users.”

In fact, the outdoor unit requires just 35% of the footprint of a conventional precision air-conditioning condenser and operation is also much quieter. Since the compressor is located in the outdoor unit, no noise emissions and no additional heat are generated in the technical room.

With the provision of the standardised EC Tower and inverter-controlled outdoor condensing units, delivery is also much faster at around two weeks. A wide range of accessories come as standard, including: fault indicators, fire shut down, common alarm, electric heating, EC compressor and much more.