Please select your country

STULZ worldwide

Interoute

  • Interoute

  • United Kingdom, London

  • CyberAir 3 with Direct Free Cooling

  • PUE <1.4

  • 1,400 kW

  • Lowering the Carbon Footprint

The Customer

Interoute (Vtesse) Cirrus Services Limited, founded in 2009, is a modern service company with the vision to provide a new type of commercial data center solutions. As a sister company of Vtesse Networks Limited, Vtesse Cirrus is located in Hoddesdon, just about 34 km North of the City of London. Meeting the requirements of the Tier III+ standard, the Vtesse Cirrus Data Center embodies an energy efficient, reliable and secure Co-Location facility on 30,000 ft². Due to the usage of top quality brands for support equipment and high standard fire detection the customer consistently experiences high levels of service availability.

The challenge
Our solution
The result
Our product

The second highest operating cost of running a data center typically is the cost of air conditioning, right next to the IT servers themselves. This emphasizes the importance of installing an energy efficient cooling system – both, for the competiveness in a highly competitive market and for the environment. 

 

The goal of Vtesse Cirrus is to keep its carbon footprint as low as possible and enhance the corporate responsibility to the environment by setting a PUE (Power Usage Effectiveness) target of less than 1.4. PUE is the ratio of the total energy used by a data center facility to the energy delivered to the IT-equipment. 

Vtesse Cirrus decided a direct outside air Free Cooling system would be the technology that satisfies the needs for the data center the best. The decision was made after a comparison of the additional capital expenditure with the lower operating cost of the various technologies. In addition to that, a cooling system has to be tailored to fit the existing building. Vtesse Cirrus decided that a Free Cooling system proposed by STULZ would satisfy the cooling requirement and reduce the operating cost. The greatest challenge was to design a ductwork system, in the existing building, that was capable of handling the vast quantities of outside air and corresponding exhaust air. The requirements are met by the STULZ CyberAir 3 downflow direct expansion (DX) computer room air conditioning with FreeCool Plenum (FCP).

The CyberAir 3 in combination with the FCP automatically controls the proportions of outside air (depending on the temperature outside) to keep the inside temperature at recommended 27°C. This allows the system to operate without the energy requiring DX compressor most of the year, saving up to 80 % of the energy consumption required for cooling the data center. The remaining time, the compressors often work at part load since the demand for compressors generally is low due to the usage of Free Cooling outside air. The FCP has ductwork connections to outside air supplying air with a constant temperature from beneath the servers and returning it from the ceiling void. The ductwork system is implemented in the service corridors between customer suites. 

The STULZ Free Cooling system is a major contributor to meet Vtesse Cirrus' target of achieving a PUE of less than 1.4. The low energy cooling system reduced the costs for energy, therefore in reduced rates for hosting services and enhancing the company's competitiveness. Furthermore, the environment benefits through the smaller carbon footprint. 

This "green thought" becomes more and more important and the clients can be ensured that they co-locate in an energy efficient data center.

 

 

CyberAir 3PRO DX

The CyberAir 3PRO DX room air conditioner is the result of more than three decades of experience with projects around the world, and is the logical next step in the development of the successful CyberAir 3 series. To achieve maximum cooling capacity with a minimal footprint while promising you maximum potential savings, these HVAC system units are more adaptable than any other precision air conditioning unit on the market.

 

To the Product

Individual solutions with STULZ

You are looking for an individually configured solution for the efficient cooling of your project?

Our qualified experts will be happy to support you with an in-depth analysis and competent advice.

Get in contact