At STULZ, expertise is far more than just a word – it is a tangible concept embodied by our superbly well-trained and coordinated team of consultants, backed by many years of project experience.
When we set out to find optimum air-conditioning solutions, we take multiple factors into account, including operating costs, energy efficiency and statutory requirements such as Austria’s F-Gas Ordinance, all of which can have a significant impact on project planning. Here, it is important to have a partner on your side that is capable of providing the right technical solution, backed by many years of experience and a flawless level of system expertise.
Analysis
Type of building? New build? Conversion? Central or remote cooling? Budget? Prior to every project, we ask the right questions, and we take time to conduct a thorough inventory – and we analyze needs on the basis of your stipulations.
Support
Better planning is the outcome of knowing more! STULZ supports you with professional know-how and interdisciplinary dialogue:
- Online service portal with download archive, technical documentation, information material
- Support at the commissioning stage
- Support on the construction site
- Comprehensive network of specialist HVAC companies
Future-proof premium solutions
STULZ is one of the world’s leading system suppliers for air-conditioning technology, able to provide the right system solution for a wide range of industry requirements. Today, a growing number of customers are benefiting from this. In future it will no longer be a question of which individual air-conditioning unit should be used – but rather of finding the best overall solution for any given task. You can find an initial overview of our portfolio here. If you have any detailed questions, please do not hesitate to contact us personally.
Leading-edge quality that fits into every climate concept
Mitsubishi Heavy Industries is committed to creating high-quality room climate systems right across the performance range. In Austria, STULZ AUSTRIA is the exclusive sales partner for the room climate systems made by Mitsubishi Heavy Industries. This means you have choice as a building services planner in any given project – and we can enable you to implement your room climate concept to the highest possible standards. Mitsubishi Heavy Industries products provide the flexible scalability to suit requirements ranging from simple to complex. Its broad portfolio assures you of the optimum climate control system for absolutely any performance rating.

Optimum control to boost energy efficiency
S-Klima developed its open-loop and feedback control components specifically for the German market with the aim of making air-conditioning systems even more economical, convenient and safe to operate. The hardware and software of the CompTrol series are examples of that. This modular series can provide an appropriate system for every task, from local stand-alone solutions to integration into existing building management systems – all of which can be operated conveniently via browser or app.

Ultimate reliability for your air-conditioning project
Water transports heat 3,500 times better than air. The STULZ Explorer range of cold-water generators was designed to achieve ultimate standards of reliability. These units operate at any local temperature profile to maximum efficiency, 24 hours a day, 365 days a year – making them especially well-suited to industrial and comfort climate applications. The great flexibility of this state-of-the-art budget-oriented technology portfolio is the perfect solution to suit a great many customer requirements. The STULZ Explorer series also complies with the limits specified in ErP 2018.

Automatic optimization of efficiency for sensitive climates
STULZ has developed and produced precision air-conditioning systems for data centers for over 50 years. These many years of experience are evident in every single CyberAir 3PRO air-conditioning unit. No precision air-conditioning system can offer greater flexibility – nor can they be tailored as accurately to suit any project requirement.

All-in-one air-conditioning for Industry 4.0 projects
Industry 4.0 involves the close networking of production with the very latest of information and communication technologies. This in turn means that many companies need to have yet more computing capacity in local networks as well as directly at each workplace. With its Micro DC, STULZ is able to provide a comprehensive turn-key solution in a single device. The all-in-one principle makes planning very simple and clear to follow because Micro DC incorporates all you need right from the outset: rack, cable management, cooling operation, UPS, power supply, environmental monitoring and firefighting.
Maximum efficiency as a complete turnkey climate solution.
Air-conditioning concepts for company areas with elevated demands on temperature control such as data centers, technical centers and industrial plants are required where operational reliability and cooling are essential. Depending on the application and location, the CyberHandler 2 minimizes operating costs and achieves pPUE values of up to 1.02 through a combination of highly efficient indirect evaporative cooling and state-of-the-art components.

Maximum efficiency as a complete turnkey climate solution.
Air-conditioning concepts for company areas with elevated demands on temperature control such as data centers, technical centers and industrial plants are required where operational reliability and cooling are essential. Depending on the application and location, the CyberHandler 2 minimizes operating costs and achieves pPUE values of up to 1.02 through a combination of highly efficient indirect evaporative cooling and state-of-the-art components.

Full control for the air-conditioning of buildings
With regard to building automation, it is important to view and compare properties in a uniform manner across multiple locations. With STULZ Digitronic Software, you have the backing of a partner that uses innovative solutions for infrastructure management to achieve three objectives: more efficient use of energy within buildings, a reduction in operating costs and the conservation of resources. This software solution helps operators to adapt their air-conditioning needs dynamically to suit demand at any given time, and to identify hidden potential for saving energy. In addition, this software supports a large number of industry-standard protocols, resulting in a higher-level system that can display and evaluate a wide range of information.

Bespoke humidification for optimum air quality
From exhibition rooms to clean rooms, STULZ has been one of the pioneers in air humidification for three decades. With STULZ UltraSonic humidification systems, you can achieve an ideal, customized solution in every case as part of planning for the delivery of building services. A solution that ensures optimum processes and high quality standards. Low energy costs mean that these durable units pay for themselves within a short time.

CO2 heat pump for future-proof generation of hot water
The Q-ton range of air-to-water heat pumps with natural CO2 refrigerant are the solution for industrial applications that run on environmentally friendly energy systems. These innovative air-to-water heat pumps absorb heat from ambient air and use it quickly and efficiently to generate hot water. Interesting for building services planners: the natural refrigerant R744 protects the ozone layer (ODP = 0), has the lowest global warming potential (GWP = 1) and an efficiency of COP = 4.3 – and is not required to comply with Austria’s F-Gas Ordinance. Consequently, Q-ton helps to prevent carbon dioxide emissions and significantly reduces CO2 emissions, especially for businesses and organizations that require large volumes of hot water.
Your benefits
- Provision of hot water (60°C to 90°C) even at ambient temperatures of -25°C
- 100% power rating, even at ambient temperatures from as low as -7°C
- The highest power rating coefficient in the sector (COP of 4.3 in the mid-season)
- Massive reduction in CO2 emissions
- Global Warming Potential (GWP) = 1
- Ozone Depletion Potential (ODP) = 0
- Extended and easy-to-use touchscreen LCD monitor
- User-friendly schedule production and one-handed refill process
- High-quality robust technology
- Long service life
- No refrigerant certificate needed